MCD_Toolbox installing problem: Can't see the Toolbox blocksets in Simulink Library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCD_Toolbox installing problem: Can't see the Toolbox blocksets in Simulink Library

1,514 Views
xinyuwang
Contributor I

Hello, NXP engineers

I am trying to use Toolbox for my project. After running  mbd_pnt_path, the result is successful. as the capture:

image004(06-06-15-45-57).png

But I can not find the blockset in simulink bowser:

image005(06-06-15-45-57).png

thanks!

Owen

Tags (1)
2 Replies

1,452 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Owen, 

Please open the Simulink Library Browser and click on F5 to refresh the list.

Usually the Simulink should display this message and should allow you to fix the problem:

1.JPG

Then you should select: Generate Repositories in memory

1.JPG

Hope this helps!

Daniel

1,452 Views
xinyuwang
Contributor I

thanks for your help. it is helpful.

Owen

0 Kudos
Reply