MCD_Toolbox installing problem: Can't see the Toolbox blocksets in Simulink Library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCD_Toolbox installing problem: Can't see the Toolbox blocksets in Simulink Library

1,503 次查看
xinyuwang
Contributor I

Hello, NXP engineers

I am trying to use Toolbox for my project. After running  mbd_pnt_path, the result is successful. as the capture:

image004(06-06-15-45-57).png

But I can not find the blockset in simulink bowser:

image005(06-06-15-45-57).png

thanks!

Owen

标记 (1)
2 回复数

1,441 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Owen, 

Please open the Simulink Library Browser and click on F5 to refresh the list.

Usually the Simulink should display this message and should allow you to fix the problem:

1.JPG

Then you should select: Generate Repositories in memory

1.JPG

Hope this helps!

Daniel

1,441 次查看
xinyuwang
Contributor I

thanks for your help. it is helpful.

Owen

0 项奖励
回复