MCD_Toolbox installing problem: Can't see the Toolbox blocksets in Simulink Library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCD_Toolbox installing problem: Can't see the Toolbox blocksets in Simulink Library

1,529件の閲覧回数
xinyuwang
Contributor I

Hello, NXP engineers

I am trying to use Toolbox for my project. After running  mbd_pnt_path, the result is successful. as the capture:

image004(06-06-15-45-57).png

But I can not find the blockset in simulink bowser:

image005(06-06-15-45-57).png

thanks!

Owen

タグ(1)
2 返答(返信)

1,467件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Owen, 

Please open the Simulink Library Browser and click on F5 to refresh the list.

Usually the Simulink should display this message and should allow you to fix the problem:

1.JPG

Then you should select: Generate Repositories in memory

1.JPG

Hope this helps!

Daniel

1,467件の閲覧回数
xinyuwang
Contributor I

thanks for your help. it is helpful.

Owen

0 件の賞賛
返信