MBDT with Functional Safety ISO26262.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT with Functional Safety ISO26262.

Jump to solution
2,609 Views
djdq
Contributor I

Dear MBDT Team, currently I am working on a BMW project,which requires functional safety ASIL-B, with s32k144.  It is highly recommended to work in model based way instead of hand-written codes, because of the constrains from iso26262.  S32k14x family do support 26262, and those safety related features, such as ECC and SCST, are also available at S32DS. However couldn't be found at MBDT... Are you working on that? When yes, when could it be released? Thanks.

Jiabin

0 Kudos
Reply
1 Solution
2,543 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Jiabin, 

For the moment we do not have support for those peripherals. Typically, for new functionality there is an approval process to go into pipeline of the development team. Can you get in touch with your local NXP representative and ask for such feature requests ?

yiling_zhang‌ just FYI

Best regards,
Daniel

View solution in original post

0 Kudos
Reply
2 Replies
2,544 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Jiabin, 

For the moment we do not have support for those peripherals. Typically, for new functionality there is an approval process to go into pipeline of the development team. Can you get in touch with your local NXP representative and ask for such feature requests ?

yiling_zhang‌ just FYI

Best regards,
Daniel

0 Kudos
Reply
2,543 Views
djdq
Contributor I

hello Daniel, thanks for the reply! I will contact NXP local team. 

0 Kudos
Reply