MBDT with Functional Safety ISO26262.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT with Functional Safety ISO26262.

ソリューションへジャンプ
2,600件の閲覧回数
djdq
Contributor I

Dear MBDT Team, currently I am working on a BMW project,which requires functional safety ASIL-B, with s32k144.  It is highly recommended to work in model based way instead of hand-written codes, because of the constrains from iso26262.  S32k14x family do support 26262, and those safety related features, such as ECC and SCST, are also available at S32DS. However couldn't be found at MBDT... Are you working on that? When yes, when could it be released? Thanks.

Jiabin

0 件の賞賛
返信
1 解決策
2,534件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Jiabin, 

For the moment we do not have support for those peripherals. Typically, for new functionality there is an approval process to go into pipeline of the development team. Can you get in touch with your local NXP representative and ask for such feature requests ?

yiling_zhang‌ just FYI

Best regards,
Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,535件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Jiabin, 

For the moment we do not have support for those peripherals. Typically, for new functionality there is an approval process to go into pipeline of the development team. Can you get in touch with your local NXP representative and ask for such feature requests ?

yiling_zhang‌ just FYI

Best regards,
Daniel

0 件の賞賛
返信
2,534件の閲覧回数
djdq
Contributor I

hello Daniel, thanks for the reply! I will contact NXP local team. 

0 件の賞賛
返信