MBDT with Functional Safety ISO26262.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MBDT with Functional Safety ISO26262.

跳至解决方案
1,774 次查看
djdq
Contributor I

Dear MBDT Team, currently I am working on a BMW project,which requires functional safety ASIL-B, with s32k144.  It is highly recommended to work in model based way instead of hand-written codes, because of the constrains from iso26262.  S32k14x family do support 26262, and those safety related features, such as ECC and SCST, are also available at S32DS. However couldn't be found at MBDT... Are you working on that? When yes, when could it be released? Thanks.

Jiabin

0 项奖励
回复
1 解答
1,708 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Jiabin, 

For the moment we do not have support for those peripherals. Typically, for new functionality there is an approval process to go into pipeline of the development team. Can you get in touch with your local NXP representative and ask for such feature requests ?

yiling_zhang‌ just FYI

Best regards,
Daniel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,709 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Jiabin, 

For the moment we do not have support for those peripherals. Typically, for new functionality there is an approval process to go into pipeline of the development team. Can you get in touch with your local NXP representative and ask for such feature requests ?

yiling_zhang‌ just FYI

Best regards,
Daniel

0 项奖励
回复
1,708 次查看
djdq
Contributor I

hello Daniel, thanks for the reply! I will contact NXP local team. 

0 项奖励
回复