MBDT for mpc574x can not run.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT for mpc574x can not run.

Jump to solution
6,539 Views
hongjinzeng
Contributor IV

Hi everyone,

      Today,I install the MBDT for mpc574x. According to the indicate, I generate the lic file.Then I open the gpio_mpc574x.mdl,click the build button,the error appearance.Can you help me solve the problem?

捕获.PNG

Tags (1)
0 Kudos
Reply
1 Solution
6,339 Views
constantinrazva
NXP Employee
NXP Employee

Hello hongjinzeng‌,

Can you open a command prompt on your computer and run the following command

vol

pastedImage_4.png

and tell us if the Volume Serial Number matches the one from the license file?

 

pastedImage_6.png

(this is from license.dat file)

 

Kind regards,

Razvan.

View solution in original post

7 Replies
6,340 Views
constantinrazva
NXP Employee
NXP Employee

Hello hongjinzeng‌,

Can you open a command prompt on your computer and run the following command

vol

pastedImage_4.png

and tell us if the Volume Serial Number matches the one from the license file?

 

pastedImage_6.png

(this is from license.dat file)

 

Kind regards,

Razvan.

6,339 Views
hongjinzeng
Contributor IV

sorry, the Volume Serial Number is different.

0 Kudos
Reply
6,339 Views
constantinrazva
NXP Employee
NXP Employee

Hi,

I was just about to point that out - try generating the license again and come back here if you still face issues.

Kind regards,

Razvan.

0 Kudos
Reply
6,339 Views
hongjinzeng
Contributor IV

After I add the MBDT lic file's address to the environment variables like this    LM_LICENSE_FILE = C:\Users\ZengHongJing\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_MPC57xx\lic\license.lic

The project build successful.

0 Kudos
Reply
6,339 Views
constantinrazva
NXP Employee
NXP Employee

Hello hongjinzeng‌,

I will investigate why this is happening - but thank you for letting us know about this workaround.

Kind regards,

Razvan. 

0 Kudos
Reply
6,339 Views
hongjinzeng
Contributor IV

I try to generate the license again,but the issuse also remain.

捕获.PNG

0 Kudos
Reply
6,339 Views
hongjinzeng
Contributor IV

捕获.PNG

捕获1.PNG

The Volume Serial Number is same ,but also the error will appearance.

0 Kudos
Reply