MBDT for Simulink - Generate Licenses - What to Put in Name Field?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT for Simulink - Generate Licenses - What to Put in Name Field?

ソリューションへジャンプ
1,556件の閲覧回数
rsating
Contributor III

When creating a license for the NXP Model Based Design Toolbox for Simulink, we have to create a license on the NXP website as shown below in the attached screenshot.  What is the purpose of the "Name" field?  Name of the machine?  Or something else?  Is entry in the field optional? Or required for activation to succeed?

Following the link "Instructions for finding your host ID details are available here." did not help answer the question.

Thanks

NXP_MBDT_Generate-Licenses_fields.png

0 件の賞賛
返信
1 解決策
1,544件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @rsating ,

You can type any name there. I think the purpose of that field is to add a brief text note to your license. Just the Disk Serial number has to be the correct one.

Hope this helps,

Marius

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,545件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @rsating ,

You can type any name there. I think the purpose of that field is to add a brief text note to your license. Just the Disk Serial number has to be the correct one.

Hope this helps,

Marius

0 件の賞賛
返信