MBDT for Simulink - Generate Licenses - What to Put in Name Field?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MBDT for Simulink - Generate Licenses - What to Put in Name Field?

跳至解决方案
1,351 次查看
rsating
Contributor III

When creating a license for the NXP Model Based Design Toolbox for Simulink, we have to create a license on the NXP website as shown below in the attached screenshot.  What is the purpose of the "Name" field?  Name of the machine?  Or something else?  Is entry in the field optional? Or required for activation to succeed?

Following the link "Instructions for finding your host ID details are available here." did not help answer the question.

Thanks

NXP_MBDT_Generate-Licenses_fields.png

0 项奖励
回复
1 解答
1,339 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @rsating ,

You can type any name there. I think the purpose of that field is to add a brief text note to your license. Just the Disk Serial number has to be the correct one.

Hope this helps,

Marius

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,340 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @rsating ,

You can type any name there. I think the purpose of that field is to add a brief text note to your license. Just the Disk Serial number has to be the correct one.

Hope this helps,

Marius

0 项奖励
回复