MBDT for S32G274A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBDT for S32G274A

1,879 Views
puravp
Contributor II

Hey guys, 

I am new to NXP boards so please bear my noob questions.

 Is there a MBDT for S32G274A board? I would like to perform PIL simulation using Simulink

Thanks

Purav

0 Kudos
Reply
2 Replies

1,877 Views
brianmckay
Contributor III

Try the HCP package at link below. Supports PIL simulation on S32G2xx: 
https://www.mathworks.com/matlabcentral/fileexchange/101378-nxp-support-package-hcp

 

Cheers,

-Brian

1,849 Views
puravp
Contributor II

I tried that, and followed the steps. During writing linux image on sd card, I am receiving following error:

 

>> mbd_hcp.setup.guiSetupToolbox
Error using mbd_hcp.setup.WindowsHardwareModule/getFirmwareWritePercentComplete
Error writing to the memory card: An error occurred while writing to the SD card. The request could not be performed because of an I/O device error.


Error in mbd_hcp.setup.guiSetupToolbox/WriteImageWriteButtonPushed

Error using matlab.ui.control.internal.controller.ComponentController/executeUserCallback (line 427)
Error while evaluating Button PrivateButtonPushedFcn.

 

Any idea?

0 Kudos
Reply