MBDT build and flash error on RDVCU5775B-EVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT build and flash error on RDVCU5775B-EVM

433件の閲覧回数
RegulusCheng
Contributor III

Hi, Marius @mariuslucianand 

I have a new problem with using MBDT for the RDVCU5775EVM board, and I need your help.

The background is: I accidentally pressed the reset button when the MBDT toolbox was downloading the program onto the board and then the download failed and the flash seems blocked (It stocked on CRC verifying step when using S32DS to flash). I have met this before, and I erased the flash using PKGPPCNEXUS according to this thread: 已解决: Unable to start debug session on MPC5748G board. download stops at 98% - NXP Community

It works and I can download elf files using  S32DS to flash the board. However, I can not use the MBDT toolbox to download anymore. The progress stocks on the "init" step and then a window shows I have lost connection with the board.

I have flashed the bootloader again after erasing the flash, but it not work. Do you have any suggestions? Or do you know who I can ask for help now?

By the way, I can accept using S32DS to download elf file which is generated by the MBDT toolbox, but the program disappears after pushing the reset button, and I have to flash again, how can I keep the program after pushing reset, when using S32DS to flash the program?

 

Waiting for your reply,

Regulus

 

0 件の賞賛
返信
0 返答(返信)