MBDT Toolbox SPI transfer does not correctly issue multi-byte transfers (bug report, critical)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MBDT Toolbox SPI transfer does not correctly issue multi-byte transfers (bug report, critical)

跳至解决方案
10,852 次查看
glenndoiron
Contributor II

Using : MBDToolbox 4.2.1,with hotfix for register access blocks.
Using: S32K144 LQFP-100, on proprietary hardware board

When setting the LPSPI_Config block to have a transfer size of 8 bits, I can pass an array of one UINT8 to the LPSPI_Master_Transfer block and the SPI bus correctly outputs the byte of data.

When I set the transfer size to 32 bits, and pass an array of 4 UNIT8 bytes, there is no SPI activity.

I have tracked this down to the generated code for the block.  With a 32 bit  wide transfer, the generated code is

/* S-Function (lpspi_s32k_master_transfer): '<Root>/LPSPI_Master_Transfer' */
{
/* Update the peripheral CS to select the slave you want to send data to */
LPSPI_DRV_SetPcs(1, LPSPI_PCS3, LPSPI_ACTIVE_LOW);

/* Send data */
LPSPI_DRV_MasterTransferBlocking(1,
&JVCB3_TEST_TOP_B.TmpSignalConversionAtLPSPI_Mast[0],
&JVCB3_TEST_TOP_B.LPSPI_Master_Transfer[0], 1, 50);
}

The problem is argument 4 of LPSPI_DRV_MasterTransferBlocking().  It should be 4, not one.  I went through the pain of converting the test model to a compiling S32DS project, and manually changing this to 4 and compiling it produces the expected SPI transfers.

 

0 项奖励
回复
1 解答
10,610 次查看
stefancinipeanu
NXP Employee
NXP Employee

Hello, @gmud1234 @glenndoiron 

Sorry for the late answer! I have been investigating the issue that you have and indeed it is a bug on our side on how the transfer byte count value is computed (the 4th paramater of the LPSPI_DRV_MasterTransferBlocking function). This will be resolved as soon as possible in the next release which will be available soon.

Regards,

Stefan.

在原帖中查看解决方案

0 项奖励
回复
15 回复数
10,690 次查看
gmud1234
Contributor II

Any update ? Is it a bug, or a user issue!

 

0 项奖励
回复
10,611 次查看
stefancinipeanu
NXP Employee
NXP Employee

Hello, @gmud1234 @glenndoiron 

Sorry for the late answer! I have been investigating the issue that you have and indeed it is a bug on our side on how the transfer byte count value is computed (the 4th paramater of the LPSPI_DRV_MasterTransferBlocking function). This will be resolved as soon as possible in the next release which will be available soon.

Regards,

Stefan.

0 项奖励
回复
10,592 次查看
glenndoiron
Contributor II

Thanks for the response.

 

Glenn

0 项奖励
回复
10,832 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @glenndoiron,

The signature of the function LPSPI_DRV_MasterTransferBlocking requires that the data shall be transferred as an UINT8 array. So, if you want to send an UIN32_T value, you shall first cast that to an uint8_t * data type. The Simulink block expects such value data type and will compute automatically the size of the input array.

mariuslucianand_0-1659338755809.png

In this way, you could also send multiple bytes as a single transfer, in a combination with the Continous Transfer setting of the SPI_Config block.

mariuslucianand_1-1659339150602.png

If the transfer is not working, then the priorities of the interrupts shall be considered. When the timeout of the transfer action is computed, it uses the OSIF software component, which uses the PIT channel 3 as a timer for such computation. So the priorities of the PIT 3 > SPI > Step timer.

Hope this helps,

Marius

 

 

0 项奖励
回复
10,813 次查看
glenndoiron
Contributor II

This was tested by first sending an array of 1 UINT8 (using a 1 input mux) with a frame size of 8 bits.  This compiles and executes correctly.

I then switched to a frame size of 32 bits, and expanded the mux from 1 to 4 inputs.  Simulink reports the output of the mux which is feeding the spi block to be "uint8 (4)", however the generated code with this configuration does not issue a byte count of 4, it issues a byte count of 1.

Additionally at the time I had the baud rate set to 10,000bps.  When I manually changes the transfer size to 4 bytes, the compiled code executed without any issues.  The actual transfer would take (setup time + 3.2ms); the SPI transfer timeout should be 50mS, and the step timer is 100mS. 

 

 

0 项奖励
回复
10,808 次查看
glenndoiron
Contributor II

Note that I changed the attached model to show how I generated the 4-byte array, but forgot to change the transfer size before taking that screen capture.

0 项奖励
回复
10,786 次查看
gmud1234
Contributor II

I had/have a similar problem with data length set to 2 bytes (16 bits).

If I provide it with uint8[2], it calculates the length by dividing [2]/2 = 1, and sends nothing.

If I provide it with uint8[4], it calculates the length by dividing [4]/2 = 2,, it sends the first 2 bytes and ignores the second 2 bytes.

For 32 bit, I imagine you may need to provide it with 16 bytes, the first 4 bytes it will transmit, and ignore the other 12.

Not sure I understand what the option 'continuous transfer' does - it doesn't appear to be mentioned at all in the documentation that I have.

0 项奖励
回复
10,774 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @gmud1234 ,

The "Continous transfer" option, ensures that the CS pin is held on LOW for the entire Transfer length of n Bytes you want to send so that if you need to send 40bits of data, you put the data in a 5x uint8_t array and the selected device will "See" 40bits on data in one transfer.

@gmud1234 , @glenndoiron could you please send me one of your example models, so that I could have a look on how de example behaves?

Regards,

Marius

0 项奖励
回复
10,753 次查看
glenndoiron
Contributor II

Top level model:  JVCB3_TEST_TOP.

Change the MBD_S32K1xx_Config_Information to point to the COM port for your board (or switch to OpenSDA if you're using an evaluation board).

Go to Modelling tab and click on "Update Model".

Go to the "Apps" tab and click on Embedded Coder.

Click on "Build" and upload the model to the board.  Observe that there is no SPI communication.  Notice that the signal being fed into the LPSPI_Master_Transfer block is declared as "uint8 (4)" on the simulink model.

Navigate to the generated code at "<model root>\JVCB3_TEST_TOP_mbd_rtw\JVCB3_TEST_TOP.c"

Note on line 57:

/* Send data */
LPSPI_DRV_MasterTransferBlocking(1,
&JVCB3_TEST_TOP_B.TmpSignalConversionAtLPSPI_Master_TransferInport1[0],
&JVCB3_TEST_TOP_B.LPSPI_Master_Transfer[0], 1, 50);
}

And on line 42:

/* SignalConversion generated from: '<Root>/LPSPI_Master_Transfer' */
JVCB3_TEST_TOP_B.TmpSignalConversionAtLPSPI_Master_TransferInport1[0] =
rtb_byte_out;
JVCB3_TEST_TOP_B.TmpSignalConversionAtLPSPI_Master_TransferInport1[1] =
rtb_byte_out;
JVCB3_TEST_TOP_B.TmpSignalConversionAtLPSPI_Master_TransferInport1[2] =
rtb_byte_out;
JVCB3_TEST_TOP_B.TmpSignalConversionAtLPSPI_Master_TransferInport1[3] =
rtb_byte_out;

Navigate to JVCB3_TEST_TOP.h.

Note on line 37:

/* Block signals (default storage) */
typedef struct {
uint8_T TmpSignalConversionAtLPSPI_Master_TransferInport1[4];
uint8_T LPSPI_Master_Transfer[4]; /* '<Root>/LPSPI_Master_Transfer' */
} B_JVCB3_TEST_TOP_T;

The generated code is clearly a C array of 4 unit8's.   However LPSPI_DRV_MasterTransferBlocking in being passed a length of 1 byte.

0 项奖励
回复
10,764 次查看
gmud1234
Contributor II

Here is the model of the problem with 16bit SPI. (A model is also attached).

Where is the best place to find documentation on the SPI ? Is the underlying 'C' framework the best source of documentation ?

gmud1234_0-1659600583719.png

 

0 项奖励
回复
10,668 次查看
ruihang_wu
Contributor III

Have you tried setting the frame size to 8b in the SPI config block and sending a uint8[4] to the SPI transfer block? And of course with continuous transfer checked

0 项奖励
回复
10,640 次查看
gmud1234
Contributor II

If you set it to 8bits, it drops chip select after each transfer of 8bits. This does not work if the peripheral is expecting 16bit before dropping chip select.

0 项奖励
回复
10,616 次查看
ruihang_wu
Contributor III

I tried with 8b frame size and continuous transfer checked and it seems to work fine. I didn't connect the bus to anything so there is no reply.

This is running on the S32K144 EVB. But I have been running it on a proprietary board with the same MCU with these settings.

ruihang_wu_2-1661538385619.png

 

ruihang_wu_1-1661538113279.png

 

ruihang_wu_0-1661538075345.png

I attached the simple model if you want to compare the SPI settings.

0 项奖励
回复
10,630 次查看
glenndoiron
Contributor II

For what it's worth, the target tested SPI device in question is a PCB with a string of daisy chained 74164's and it wouldn't matter if CS is dropped between bytes or not.  But my testing was done with continuous transfers enabled.

0 项奖励
回复
10,629 次查看
glenndoiron
Contributor II

Also there are other devices on other SPI ports, which have 16-bit, 32-bit, and 64-bit frame sizes, and WILL have an issue if chip select is dropped between bytes, so its pretty important that this gets fixed

0 项奖励
回复