[MBDT,S32 DesignStudio]Code Generation and Configuration for NonAutosar - S32K312 EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MBDT,S32 DesignStudio]Code Generation and Configuration for NonAutosar - S32K312 EVB

1,283 Views
jyoti_c
Contributor II

Hi,

I am using MBDT for NXP S32K312.

I see that the S32 configuration available using MBDT is in AutosarMode which is in MCAL layer.(refer image AutosarMode.jpg) 

But am working on Bare metal coding in S32Design Studio ( under Drivers)(refer image DriverMode.jpg).

Can you help me know if I can generate code/configure for bare metal coding using MBDT(under Drivers in S32DesignStudio)?

#MBDT #S32K312 #HardwareConfiguration #Non-AUTOSAR


Thanks in Advance
Jyoti C

Tags (2)
0 Kudos
Reply
1 Reply

1,085 Views
stefancinipeanu
NXP Employee
NXP Employee

Hello @jyoti_c 

Unfortunately, Simulink blocks for accessing the S32K3 peripherals in the code generation flow are based on Real-Time Drivers MCAL layer only.  Currently, we do not support code generation on Drivers layer.

Thanks & Regards!

Stefan.

 

0 Kudos
Reply