MBDT CAN Rx Message Size

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MBDT CAN Rx Message Size

1,758 次查看
C_Zuercher_APR
Contributor III

Hi,

I'm trying to recieve a CAN Message with a data length of 1 byte, however the MBDT CAN Rx block appears to be set as a uint8(8) vector. is there a way of recieving a smaller message?

Thanks,

Crispin

0 项奖励
回复
1 回复

1,738 次查看
oliveadam
Contributor I

CAN 2.0A & 2.0B Message Frames Nodes 0 and 1 will re-transmit their messages when the bus  16 Rx/Tx Message Buffers of up to 8 bytes Data Length.

My Lowe's Life

0 项奖励
回复