MBD Toolbox : I2C module ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBD Toolbox : I2C module ?

2,429件の閲覧回数
adrienpol
Contributor II

Hello,

I was looking for an I2C block in the MBD Toolbox, but I can't find one. I was pretty sur it was supported as I read it on the main presentation of MBD Toolbox :

Model-Based Design Toolbox|NXP 

I'm using a MPC5744P, is there a trick to find an I2C block ? Or the I2C block doesn't support this µC ?

Tanks for your time,

Regards, Adrien.

0 件の賞賛
返信
2 返答(返信)

2,297件の閲覧回数
adrienpol
Contributor II

Thanks for your quick answer :smileywink:

I will use SPI for my project, but indeed, an I2C block would be great !

Regards, Adrien.

0 件の賞賛
返信

2,297件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello adrienpol‌,

Unfortunately, we do not have I2C support in the latest release of MPC574xP MBDT. We do however have SPI or UART, if that helps (see examples uart_model_pnt or dspi_model_pnt). We will add I2C support in a future release, but I can not say at this point in time when it will become available.

Hope this helps,

Razvan.

0 件の賞賛
返信