MBD [MPC5744P]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBD [MPC5744P]

1,717 Views
abdelrhman
Contributor III

How to generate XML file out of simulink-based model to build it using s32 ?
I'm using MBDT for MPC57xx Series Version  3.2.0

0 Kudos
Reply
2 Replies

1,693 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @abdelrhman ,

The ProjectInfo.xml file is automatically generated if the checkbox from the MPC574x_Config block is checked as in the screenshot below.

mariuslucianand_0-1658475902537.pngmariuslucianand_0-1658475902537.png

As additional step, you have to rename the .S files into .s file extensions and to also change is inside the .xml generated file.

You shall use the S32DS for Power Architecture V2.1.

Hope this helps,

Marius

 

0 Kudos
Reply

1,677 Views
abdelrhman
Contributor III

I tried to import the xml file of gpio_mpc574x MBD model and built the project using s32, but I got the following errors

abdelrhman_0-1658582886859.pngabdelrhman_0-1658582886859.png

 

0 Kudos
Reply