MBD [MPC5744P]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBD [MPC5744P]

1,791件の閲覧回数
abdelrhman
Contributor III

How to generate XML file out of simulink-based model to build it using s32 ?
I'm using MBDT for MPC57xx Series Version  3.2.0

0 件の賞賛
返信
2 返答(返信)

1,767件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @abdelrhman ,

The ProjectInfo.xml file is automatically generated if the checkbox from the MPC574x_Config block is checked as in the screenshot below.

mariuslucianand_0-1658475902537.png

As additional step, you have to rename the .S files into .s file extensions and to also change is inside the .xml generated file.

You shall use the S32DS for Power Architecture V2.1.

Hope this helps,

Marius

 

0 件の賞賛
返信

1,751件の閲覧回数
abdelrhman
Contributor III

I tried to import the xml file of gpio_mpc574x MBD model and built the project using s32, but I got the following errors

abdelrhman_0-1658582886859.png

 

0 件の賞賛
返信