MBD Compile Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBD Compile Error

2,253 Views
dmeng1
Contributor II

Dear Daniel:

I download a S12ZVM_Trap_Ctrl model from NXP , but when I build the model , it appears a error like belows:

pastedImage_1.png

could you tell me how to slove this error ? thanks very much .

0 Kudos
Reply
2 Replies

2,070 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

Please have a look here - at hotfix #2. That should fix your error.

Kind regards,

Razvan.

0 Kudos
Reply

2,070 Views
dmeng1
Contributor II

Hello Constantin:

Thank you very much , I have solve this problem. I want to ask you another question, when I generate the code from matlab simulink. How should I call codewarrior to compile the code . because generated code is C code, it is not a codewarrior project. I want to use codewarrior to compile the code and generate the elf or s19 file ,then flash it to MCU.  expect for your reply, thanks.

0 Kudos
Reply