License Error: -1, Model-Based Design Toolbox License Missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

License Error: -1, Model-Based Design Toolbox License Missing

3,207 Views
jaiprakash_chav
Contributor I

License Error: -1, Model-Based Design Toolbox License Missing, please go to The Model-Based Design Development Toolbox Web Site to get a free license or request a demo. Provide the following HostID: 3a18c7db.

I followed below steps:

1)  Generated license with correct Host ID

2) Saved to license.lic and placed inside lic folder

Kindly help .

0 Kudos
Reply
3 Replies

3,031 Views
kevin_kawakami
Contributor II

This works!

changing the extension of the license.dat --> license.lic

3,031 Views
kevin_kawakami
Contributor II

Hi, Admin.

Next is connect Freemaster.

Where can I get file “BLDC_ClosedLoop_s32k14x.pmp”?

I have old file but that has “Missing Symbol Definitions”

Thank you.

0 Kudos
Reply

3,031 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

For which product do you try to get the license?

Can you provide a screenshot with the file system of the installed toolbox and where you added the license?

Also try changing the extension of the license from .lic to .dat.

Hope this helps,

Marius

0 Kudos
Reply