License Error: -1, Model-Based Design Toolbox License Missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

License Error: -1, Model-Based Design Toolbox License Missing

3,238件の閲覧回数
jaiprakash_chav
Contributor I

License Error: -1, Model-Based Design Toolbox License Missing, please go to The Model-Based Design Development Toolbox Web Site to get a free license or request a demo. Provide the following HostID: 3a18c7db.

I followed below steps:

1)  Generated license with correct Host ID

2) Saved to license.lic and placed inside lic folder

Kindly help .

0 件の賞賛
返信
3 返答(返信)

3,062件の閲覧回数
kevin_kawakami
Fresh Out Contributor

This works!

changing the extension of the license.dat --> license.lic

3,062件の閲覧回数
kevin_kawakami
Fresh Out Contributor

Hi, Admin.

Next is connect Freemaster.

Where can I get file “BLDC_ClosedLoop_s32k14x.pmp”?

I have old file but that has “Missing Symbol Definitions”

Thank you.

0 件の賞賛
返信

3,062件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

For which product do you try to get the license?

Can you provide a screenshot with the file system of the installed toolbox and where you added the license?

Also try changing the extension of the license from .lic to .dat.

Hope this helps,

Marius

0 件の賞賛
返信