Issue with S32K MBDT License Installer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with S32K MBDT License Installer

3,868 Views
srikar_26
Contributor II

Hi,

I was trying to download and verify NXP S32K MBDT toolbox, I am gettin this issue.

 License Error: -1, Model-Based Design Toolbox License Missing, please go to The Model-Based Design Development Toolbox Web Site to get a free license or request a demo. Provide the following HostID.

What is HostID?

We have followed this video: https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Model-Based-Design-Toolbox-Quick-Install-G...

Thank you

Tags (2)
0 Kudos
Reply
5 Replies

3,483 Views
Nayan123
Contributor II
  • cap.PNG

Anyone please comment on how to resolve this issue?

0 Kudos
Reply

3,853 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @srikar_26 ,

The HostID is the Volume Serial Number for your volume partition.

To get this id XXXX-XXXX you have to open a Command Prompt and type the "vol" command, as below.

mariuslucianand_0-1639134665916.png

Hope this helps,

Marius

 

0 Kudos
Reply

3,822 Views
srikar_26
Contributor II

Hi,

We have generated the HostID as per the video, but we are still getting the same License error.

Thanks

0 Kudos
Reply

3,802 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @srikar_26 ,

Can you please check that the license file is located here? Please type the following command in MATLAB.

winopen(fullfile(mbd_find_s32k_root, 'lic'))

Hope this helps,

Marius

Tags (1)
0 Kudos
Reply

3,787 Views
srikar_26
Contributor II

Hi @mariuslucianand ,

The license file was located when I've given the above command. The license file extension is .lic. But still I'm facing the issue with the license error. Is there any other solution?

Thanks.

0 Kudos
Reply