Issue with S32K MBDT License Installer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue with S32K MBDT License Installer

3,870件の閲覧回数
srikar_26
Contributor II

Hi,

I was trying to download and verify NXP S32K MBDT toolbox, I am gettin this issue.

 License Error: -1, Model-Based Design Toolbox License Missing, please go to The Model-Based Design Development Toolbox Web Site to get a free license or request a demo. Provide the following HostID.

What is HostID?

We have followed this video: https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Model-Based-Design-Toolbox-Quick-Install-G...

Thank you

タグ(2)
0 件の賞賛
返信
5 返答(返信)

3,485件の閲覧回数
Nayan123
Contributor II
  • cap.PNG

Anyone please comment on how to resolve this issue?

0 件の賞賛
返信

3,855件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @srikar_26 ,

The HostID is the Volume Serial Number for your volume partition.

To get this id XXXX-XXXX you have to open a Command Prompt and type the "vol" command, as below.

mariuslucianand_0-1639134665916.png

Hope this helps,

Marius

 

0 件の賞賛
返信

3,824件の閲覧回数
srikar_26
Contributor II

Hi,

We have generated the HostID as per the video, but we are still getting the same License error.

Thanks

0 件の賞賛
返信

3,804件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @srikar_26 ,

Can you please check that the license file is located here? Please type the following command in MATLAB.

winopen(fullfile(mbd_find_s32k_root, 'lic'))

Hope this helps,

Marius

タグ(1)
0 件の賞賛
返信

3,789件の閲覧回数
srikar_26
Contributor II

Hi @mariuslucianand ,

The license file was located when I've given the above command. The license file extension is .lic. But still I'm facing the issue with the license error. Is there any other solution?

Thanks.

0 件の賞賛
返信