Is there a way to have CAN_ID as an input to the CAN send block rather than a fixed value?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there a way to have CAN_ID as an input to the CAN send block rather than a fixed value?

跳至解决方案
3,526 次查看
Poley
Contributor V

Hi, 

Instead of having a fixed value in the CAN send block

Poley_0-1620635877492.png

Can I somehow have CAN ID as an input alongside data and length?

Poley_1-1620635979002.png

The reason is I want to send messages on a different ID depending on a bitmask value (1-16) and if I could enter the ID instead, otherwise I have to make 16 versions of all my CAN outputs.

Thanks in advance!

 

 

0 项奖励
回复
1 解答
3,462 次查看
paulvlase
NXP Employee
NXP Employee

Hi @Poley and @Maciek ,

 

I attached a cumulative patch, a self-extracting archive, that contains this improvement and the previous patches from CAN FD in S32k14x EVB .

 

The steps to apply the patch:

1. Download the attached zip file and unzip it.

2. Run mbd_find_s32k_root() to get the root folder there the S32K toolbox is installed.

3. Close Matlab.

4. Open the MBDToolbox_S32K1xx_4.2.0_id_input_patch_3.exe file and extract it's contents to the root folder of the toolbox.

 

To show the ID input you have to check the "Show ID input port" option in the FCAN_Send and FCAN_Receive blocks.

paulvlase_1-1621964258862.png

 

Regards,

Paul

 

在原帖中查看解决方案

7 回复数
3,463 次查看
paulvlase
NXP Employee
NXP Employee

Hi @Poley and @Maciek ,

 

I attached a cumulative patch, a self-extracting archive, that contains this improvement and the previous patches from CAN FD in S32k14x EVB .

 

The steps to apply the patch:

1. Download the attached zip file and unzip it.

2. Run mbd_find_s32k_root() to get the root folder there the S32K toolbox is installed.

3. Close Matlab.

4. Open the MBDToolbox_S32K1xx_4.2.0_id_input_patch_3.exe file and extract it's contents to the root folder of the toolbox.

 

To show the ID input you have to check the "Show ID input port" option in the FCAN_Send and FCAN_Receive blocks.

paulvlase_1-1621964258862.png

 

Regards,

Paul

 

3,374 次查看
Poley
Contributor V

Hi @paulvlase 

I now get this message when using this patch:

Poley_0-1623239366346.png

The fix you sent seems to work perfectly I was just wondering if this new message points to an issue I haven't come across yet?

Thanks!

 

0 项奖励
回复
3,458 次查看
Poley
Contributor V

This is a huge help, thank you!

0 项奖励
回复
3,494 次查看
Poley
Contributor V

Hi @mariuslucianand 

Is this possible?

Thanks!

0 项奖励
回复
3,489 次查看
paulvlase
NXP Employee
NXP Employee

Hi @Poley ,

 

No, you can't pass the ID as an input signal. To allow you to do that, we will need to update the toolbox.

 

I can send you a patch tomorrow if you are fine with it, which you will have to apply over the toolbox.

 

Regards,

Paul

0 项奖励
回复
3,473 次查看
Maciek
Contributor V

Hi @paulvlase 

I have been writing about this issue a few months ago. We are also interested in a solution to this problem. Right now our model uses more than 150 unnecessary CAN send blocks (to send messages with various IDs) - it works fine, but the model is clumsy and more than 4000 lines of code is generated from this unnecessary blocks.

Regards

Maciek 

0 项奖励
回复
3,487 次查看
Poley
Contributor V

Hi @paulvlase 

That would be very helpful, thank you!

Will reduce my code size massively.

Thank you.

0 项奖励
回复