Is there Motor Control Toolbox for 56F84xx ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there Motor Control Toolbox for 56F84xx ?

跳至解决方案
1,870 次查看
Maciek
Contributor V

On a few PDFs available from NXP site there is a 'compatibility' section that showes all supported MCUs. In this section there is entry "56F82xx / 56F84xx". It suggests that 56F84xx are also supported by MCToolbox. But after installing MCToolbox for DSCs - release notes (in 'help' folder) list only 56F82xx devices as supported.

Is it a mistake in the presentations PDFs ?

Or maybe there is (or there will be in the near future) such support ?

Thanks for help

Maciek

标记 (2)
0 项奖励
回复
1 解答
1,649 次查看
raduivan
NXP Employee
NXP Employee

Hi Maciek,

   The current version of DSC MCToolbox is not supporting the 56F84xx family.

Best regards,

Radu

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,650 次查看
raduivan
NXP Employee
NXP Employee

Hi Maciek,

   The current version of DSC MCToolbox is not supporting the 56F84xx family.

Best regards,

Radu

0 项奖励
回复