Is there Motor Control Toolbox for 56F84xx ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there Motor Control Toolbox for 56F84xx ?

Jump to solution
1,877 Views
Maciek
Contributor V

On a few PDFs available from NXP site there is a 'compatibility' section that showes all supported MCUs. In this section there is entry "56F82xx / 56F84xx". It suggests that 56F84xx are also supported by MCToolbox. But after installing MCToolbox for DSCs - release notes (in 'help' folder) list only 56F82xx devices as supported.

Is it a mistake in the presentations PDFs ?

Or maybe there is (or there will be in the near future) such support ?

Thanks for help

Maciek

0 Kudos
Reply
1 Solution
1,656 Views
raduivan
NXP Employee
NXP Employee

Hi Maciek,

   The current version of DSC MCToolbox is not supporting the 56F84xx family.

Best regards,

Radu

View solution in original post

0 Kudos
Reply
1 Reply
1,657 Views
raduivan
NXP Employee
NXP Employee

Hi Maciek,

   The current version of DSC MCToolbox is not supporting the 56F84xx family.

Best regards,

Radu

0 Kudos
Reply