Is there Motor Control Toolbox for 56F84xx ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there Motor Control Toolbox for 56F84xx ?

ソリューションへジャンプ
2,691件の閲覧回数
Maciek
Contributor V

On a few PDFs available from NXP site there is a 'compatibility' section that showes all supported MCUs. In this section there is entry "56F82xx / 56F84xx". It suggests that 56F84xx are also supported by MCToolbox. But after installing MCToolbox for DSCs - release notes (in 'help' folder) list only 56F82xx devices as supported.

Is it a mistake in the presentations PDFs ?

Or maybe there is (or there will be in the near future) such support ?

Thanks for help

Maciek

0 件の賞賛
返信
1 解決策
2,470件の閲覧回数
raduivan
NXP Employee
NXP Employee

Hi Maciek,

   The current version of DSC MCToolbox is not supporting the 56F84xx family.

Best regards,

Radu

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,471件の閲覧回数
raduivan
NXP Employee
NXP Employee

Hi Maciek,

   The current version of DSC MCToolbox is not supporting the 56F84xx family.

Best regards,

Radu

0 件の賞賛
返信