How to use the BMS example in NXPS32K for MPC5777C-DEVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the BMS example in NXPS32K for MPC5777C-DEVB

1,223 Views
Elisay
Contributor I

As the subject, is it possible to download the BMS example available in the MBDT for NXPS32K if I already have the MBDT for MPC5777C installed? If not, will a similar example be available for 5777C?

This is the example I'm talking about: https://www.mathworks.com/videos/deploying-battery-management-system-algorithms-on-nxp-s32k-from-sim...  I understand s32k is quite different from 57xx, but there is no example BMS available in MBDToolbox_MPC57xx, which is why I wonder if I could somehow use the example in s32k and make changes and use it for MPC57xx.

Thanks much, Elisa

0 Kudos
Reply
1 Reply

1,192 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @Elisay ,

Thank you for opening this thread on the MBDT Community.

For now, we do not provide support for the Battery Cell Controllers for MPC. However, you can achieve such functionality using the custom code insertions, as I've described in this article https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-...

For BMS, please also check rather it is more appropriate for your application the following setup: https://www.nxp.com/design/designs/mpc5775b-bms-and-vcu-reference-design:RDVCU5775EVM

Hope this helps,

Marius

0 Kudos
Reply