How to use the BMS example in NXPS32K for MPC5777C-DEVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use the BMS example in NXPS32K for MPC5777C-DEVB

1,143件の閲覧回数
Elisay
Contributor I

As the subject, is it possible to download the BMS example available in the MBDT for NXPS32K if I already have the MBDT for MPC5777C installed? If not, will a similar example be available for 5777C?

This is the example I'm talking about: https://www.mathworks.com/videos/deploying-battery-management-system-algorithms-on-nxp-s32k-from-sim...  I understand s32k is quite different from 57xx, but there is no example BMS available in MBDToolbox_MPC57xx, which is why I wonder if I could somehow use the example in s32k and make changes and use it for MPC57xx.

Thanks much, Elisa

0 件の賞賛
返信
1 返信

1,112件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @Elisay ,

Thank you for opening this thread on the MBDT Community.

For now, we do not provide support for the Battery Cell Controllers for MPC. However, you can achieve such functionality using the custom code insertions, as I've described in this article https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/How-to-use-your-own-C-code-in-our-Toolbox-...

For BMS, please also check rather it is more appropriate for your application the following setup: https://www.nxp.com/design/designs/mpc5775b-bms-and-vcu-reference-design:RDVCU5775EVM

Hope this helps,

Marius

0 件の賞賛
返信