How to use dual MC33664 loopback alongside UJA1132 SBC with only the 3 SPI busses on the S32K1?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use dual MC33664 loopback alongside UJA1132 SBC with only the 3 SPI busses on the S32K1?

1,035 次查看
Poley
Contributor V

Hi all,

 

I am designing a BMS for a one-off use case with the S32K148 before moving to the S32K3. I want to use the S32K1 MBDT so looking at the MC33664 for the TPL control and MC33771C's for the cell monitor boards.

 

I want to have a loopback system running with 2 x MC33664 so that it protects for a single disconnect/failure in the TPL loop harness.For the loopback it looks like I need all 3 SPI busses for this, is that correct? If so, because this changes the SPI the 48b transfer size, will I be able to share this SPI bus with the UJA1132 SBC? I want to use the UJA as my power supply for the uC stepping down from a 12V supply voltage. Looking at the UJA examples it always uses 8b SPI transfer size. I would want to put this on the common TX bus for the 2 TPL ports to keep both TPL RX lines on their own.

 

Is this possible? Or is there a workaround for this if not?

 

Thanks in advance!

 

 

标记 (4)
0 项奖励
回复
1 回复

1,012 次查看
Poley
Contributor V

@mariuslucianandIs this possible or should I not use the UJA1132HW/FD/5V/4Y like the S32K148 EVB?

0 项奖励
回复