How to use Rappid bootloader with S12ZVML-MINIBRD kit ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use Rappid bootloader with S12ZVML-MINIBRD kit ?

2,154 次查看
Maciek
Contributor V

I've flashed S12ZVM.rbf file into the board (and configured COM port and 'download after build' in model Configuration parameters). When I'm trying to build and download Simulink model into the board - I get the following error message: 'CCP Communication Error. Loss Communicatin with CCP MCU. Please cycle power and try again." 

How to slove this problem - I want to check PIL with this kit ?

Does the Rappid bootloader work with UART1 (which is accessible via USB on this board) ?

Thanks

Maciek 

标记 (1)
1 回复

1,853 次查看
raduivan
NXP Employee
NXP Employee

Hi Maciek,

   Try to rest the board after writing the rbf, using the reset switch or by removing the power supply.

   Press 'OK' button in less than 5 seconds.

Regards,

Radu

0 项奖励
回复