How to update from v4.1.0 to v.4.2.0?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to update from v4.1.0 to v.4.2.0?

跳至解决方案
1,233 次查看
juliana_rojas30
Contributor III

Hello there!

I have a pretty basic question. I want to update my toolbox from V4.1.0 to v4.2.0, but I am not sure which file to download or how to do it. I see the files in the image below, which one should I use?

img1.PNG

Should I uninstall the previous installation and start from zero with the new one? Or can I install it on the old version? How should I proceed? Some help would be really appreciated!

Thank you all!

0 项奖励
回复
1 解答
1,217 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @juliana_rojas30 ,

The best way is to uninstall the 4.1.0 version. For that, you can delete the files from the AddOns folder on the Matlab version and then reset Matlab's path to default.

Then you can install the 4.2.0. You can do this directly from Matlab's Add-Ons following the instructions there. 

mariuslucianand_0-1610365981992.png

Hope this helps,

Marius

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,218 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @juliana_rojas30 ,

The best way is to uninstall the 4.1.0 version. For that, you can delete the files from the AddOns folder on the Matlab version and then reset Matlab's path to default.

Then you can install the 4.2.0. You can do this directly from Matlab's Add-Ons following the instructions there. 

mariuslucianand_0-1610365981992.png

Hope this helps,

Marius

0 项奖励
回复