How to update from v4.1.0 to v.4.2.0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to update from v4.1.0 to v.4.2.0?

ソリューションへジャンプ
1,284件の閲覧回数
juliana_rojas30
Contributor III

Hello there!

I have a pretty basic question. I want to update my toolbox from V4.1.0 to v4.2.0, but I am not sure which file to download or how to do it. I see the files in the image below, which one should I use?

img1.PNG

Should I uninstall the previous installation and start from zero with the new one? Or can I install it on the old version? How should I proceed? Some help would be really appreciated!

Thank you all!

0 件の賞賛
返信
1 解決策
1,268件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @juliana_rojas30 ,

The best way is to uninstall the 4.1.0 version. For that, you can delete the files from the AddOns folder on the Matlab version and then reset Matlab's path to default.

Then you can install the 4.2.0. You can do this directly from Matlab's Add-Ons following the instructions there. 

mariuslucianand_0-1610365981992.png

Hope this helps,

Marius

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,269件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @juliana_rojas30 ,

The best way is to uninstall the 4.1.0 version. For that, you can delete the files from the AddOns folder on the Matlab version and then reset Matlab's path to default.

Then you can install the 4.2.0. You can do this directly from Matlab's Add-Ons following the instructions there. 

mariuslucianand_0-1610365981992.png

Hope this helps,

Marius

0 件の賞賛
返信