How to measure the Phase Voltage?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to measure the Phase Voltage?

跳至解决方案
2,069 次查看
jiangfeng
Contributor III

Dear Daniel:

Which pin is used to detect the Phase Voltage  in the following figure? HS0,HS1,and HS2?

pastedImage_1.png

Besides, Is the phase voltage described above correspond to Ua,Ub and Uc in the flowing figure?  Thank you very much ,my friend.

pastedImage_2.png

标签 (1)
1 解答
1,879 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi jiangfeng‌,

I presume you need it for the BLDC sersorless drive based on phase BackEMF zero crossing. At each commutation phase (is you use the standard 2 out 3 phase commutation technique that maximize the torque) you will need to read the HSxxx that corresponds to the un-powered phase. You will need to implement your own logic algorithm to read and update the phase voltage of each phase.

In case of PMSM it is not very helpful since since by default you know/control the amount of voltage that you apply to the motor. Overall in this case might be helpful to know if a transistor is broken.

And, yes - it corresponds to Ua/Ub/Uc phase voltages.

Hope this helps!

Daniel

在原帖中查看解决方案

1 回复
1,880 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi jiangfeng‌,

I presume you need it for the BLDC sersorless drive based on phase BackEMF zero crossing. At each commutation phase (is you use the standard 2 out 3 phase commutation technique that maximize the torque) you will need to read the HSxxx that corresponds to the un-powered phase. You will need to implement your own logic algorithm to read and update the phase voltage of each phase.

In case of PMSM it is not very helpful since since by default you know/control the amount of voltage that you apply to the motor. Overall in this case might be helpful to know if a transistor is broken.

And, yes - it corresponds to Ua/Ub/Uc phase voltages.

Hope this helps!

Daniel