How to measure the Phase Voltage?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to measure the Phase Voltage?

ソリューションへジャンプ
2,081件の閲覧回数
jiangfeng
Contributor III

Dear Daniel:

Which pin is used to detect the Phase Voltage  in the following figure? HS0,HS1,and HS2?

pastedImage_1.png

Besides, Is the phase voltage described above correspond to Ua,Ub and Uc in the flowing figure?  Thank you very much ,my friend.

pastedImage_2.png

ラベル(1)
1 解決策
1,891件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi jiangfeng‌,

I presume you need it for the BLDC sersorless drive based on phase BackEMF zero crossing. At each commutation phase (is you use the standard 2 out 3 phase commutation technique that maximize the torque) you will need to read the HSxxx that corresponds to the un-powered phase. You will need to implement your own logic algorithm to read and update the phase voltage of each phase.

In case of PMSM it is not very helpful since since by default you know/control the amount of voltage that you apply to the motor. Overall in this case might be helpful to know if a transistor is broken.

And, yes - it corresponds to Ua/Ub/Uc phase voltages.

Hope this helps!

Daniel

元の投稿で解決策を見る

1 返信
1,892件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi jiangfeng‌,

I presume you need it for the BLDC sersorless drive based on phase BackEMF zero crossing. At each commutation phase (is you use the standard 2 out 3 phase commutation technique that maximize the torque) you will need to read the HSxxx that corresponds to the un-powered phase. You will need to implement your own logic algorithm to read and update the phase voltage of each phase.

In case of PMSM it is not very helpful since since by default you know/control the amount of voltage that you apply to the motor. Overall in this case might be helpful to know if a transistor is broken.

And, yes - it corresponds to Ua/Ub/Uc phase voltages.

Hope this helps!

Daniel