How to go to the following path as shown in Quick start guide

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to go to the following path as shown in Quick start guide

2,100件の閲覧回数
sutter_zhou
NXP Employee
NXP Employee

sutter_zhou_0-1619703546511.png

 

0 件の賞賛
返信
3 返答(返信)

2,091件の閲覧回数
sutter_zhou
NXP Employee
NXP Employee

I'm not talking about the simulink library page. It is the left side of this picture that makes people confused. People need to navigate to a specific path to see this folder structure.

sutter_zhou_0-1619706277727.png

 

0 件の賞賛
返信

2,076件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @sutter_zhou,

Sorry, my bad! All the MBDT toolboxes are installed in the MATLAB AddOns specific folder, which may differ for each user (everyone can select his own). To find your own or to change the default one, go to MATLAB -> Preferences and under Add-Ons you may find the toolbox location.

mariuslucianand_0-1619723869774.png

 

But, once the I.MXRT toolbox has been installed, you can type the following command in MATLAB's Command window: cd(mbd_find_imxrt_root) and this will change the Current Workspace to the one from the image.

Hope this helps,

Marius

0 件の賞賛
返信

2,094件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @sutter_zhou ,

If you refer to the Simulink library browser, you have 2 options to see it:

1. Go in any Simulink model, and you should find it under SIMULATION > Library Browser

mariuslucianand_1-1619705397065.png

2. type slLibraryBrowser in MATLAB Command Window

mariuslucianand_0-1619705258435.png

If you have installed the Toolbox but anything is missing, you can refresh the library by pressing the F5

Hope this helps,

Marius

0 件の賞賛
返信