How to dynamically change the parameter of Ld and Lq in GMCLIB_DecouplingPMSM,when the program running?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to dynamically change the parameter of Ld and Lq in GMCLIB_DecouplingPMSM,when the program running?

跳至解决方案
2,833 次查看
edenli
Contributor V

Hi Guys,

Recently,i come across a question, that is,the parameter of Lq and Ld  dynamically change ,so,i wanna realize the LD and LQ dynamically change when the program running.But i can not solve the question when use the Block of GMCLIB_DecouplingPMSM.

The attachment is my Model.

the picture shows it.

185967_185967.pngpastedImage_1.png

Original Attachment has been moved to: Decoupling.slx.zip

1 解答
2,524 次查看
paulvlase
NXP Employee
NXP Employee

Hi edenli‌,

I created the GMCLIB_DecouplingPMSM_Custom block with those two parameters from GMCLIB_DecouplingPMSM changed to input ports.

Please download the MCLIB for MPC564xL.zip, unzip it over C:\MCToolbox\rappid564xl\MCLIB for MPC564xL or replace this folder with the one from the archive.

I am waiting for your feedback,

Paul

在原帖中查看解决方案

6 回复数
2,524 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi edenli‌,

I'm afraid you can't do what you want with this NXP library block. Similar with some of the Simulink blocks if the block was not designed from the beginning to allow such changes then it simply can't be modified to accept such inputs.

In this case - the only way to tackle the problem is to implement a similar functionality with standard Simulink blocks that allows on-the-fly parameters changes.

By the way, may i ask why do you need such functionality - what is your project about to ?

Thank you!

Daniel

0 项奖励
回复
2,524 次查看
edenli
Contributor V

Hi daniel,

if you can change the S-function of Decoupling block,adding the input ports of Ld and Lq?

0 项奖励
回复
2,525 次查看
paulvlase
NXP Employee
NXP Employee

Hi edenli‌,

I created the GMCLIB_DecouplingPMSM_Custom block with those two parameters from GMCLIB_DecouplingPMSM changed to input ports.

Please download the MCLIB for MPC564xL.zip, unzip it over C:\MCToolbox\rappid564xl\MCLIB for MPC564xL or replace this folder with the one from the archive.

I am waiting for your feedback,

Paul

2,524 次查看
edenli
Contributor V

Hi Paul Vlase and daniel,

First,I am sorry so late for reply .

Thank you very much for reply!Now,i test your block about the GMCLIB_DecouplingPMSM_Custom,the result is very good.

Best Regards!

Eden Li.

0 项奖励
回复
2,524 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Eden Li, 

I guess we could do that - i need to talk with the team that provides the AMMCLIB files - because only they have the source files i need to modify.

We'll keep in touch.

Best regards,
Daniel

0 项奖励
回复
2,524 次查看
edenli
Contributor V

Hi Daniel,

Why i wanna to dynamically change the Ld and Lq? The reason is that i find the Lq and Ld changing as the Id and iq changing,and it affect the decoupling.

Daniel,if so,how to solve it abut the question ?

0 项奖励
回复