How to drive S32K144EVB correctly In Matlab simulation environment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to drive S32K144EVB correctly In Matlab simulation environment

10,638 Views
chen2021
Contributor I

Hello

In Matlab simulation environment.
I plan to use microUSB to update the model of S32K144EVB.
I updated a few examples,and there are no errors in the diagnostic viewer.
But EVB is unexecuted the model.
Could you give me some instructions? please

Two target connection settings are used(attachment:1.GPIO LED Blink(COM9).PNG & 2.GPIO LED Blink (OPEN SDA).PNG)
Installed the driver(attachment:3.DRIVER.PNG)
EVB appearance(attachment 4:.EVB.jpg)

0 Kudos
Reply
3 Replies

10,627 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @chen2021 ,

Can you please check if the Download Code after Build option is checked?

mariuslucianand_0-1626979659419.png

Hope this helps,

Marius

 

0 Kudos
Reply

10,618 Views
chen2021
Contributor I

@mariuslucianand 

Hello Marius

Thanks for your reply.

Yes, it has been checked, but still unable to successfully update the model to EVB.

Setup screenshot as attachment

 

0 Kudos
Reply

10,506 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @chen2021 ,

Can you please try to copy paste manually the .mot file form the generate folder to the mounted disk drive of the board? Maybe the OpenSDA needs an update on the board as described here https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Update-OpenSDA-Firmware-on-EVB/t...

Hope this helps,

Marius

 

 

0 Kudos
Reply