How to configure ADC using MIMXRT1170-EVK?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to configure ADC using MIMXRT1170-EVK?

跳至解决方案
2,025 次查看
esantana
Contributor III

Hi,

I am trying to set up the ADC without any interrupts but when I try to run it, it fails. I don't know if the configuration in MCUxpresso config tools is adecuated or if something is missing.

I attached the model which I am trying to compile.

Thanks in advance.

0 项奖励
回复
1 解答
1,916 次查看
stefancinipeanu
NXP Employee
NXP Employee

Hello, @esantana 

We have tested the ADC peripheral and we are not aware of any limitations. Did you try to run the ADC example on polling from MBDT IMXRT toolbox? What kind of error did you get when trying to build the application?

Usually, to use ADC in polling mode you just have to disable ADC interrupt from configuration file attached to the model, as depicted below:

stefancinipeanu_0-1673943997728.png

 

Best regards,

Stefan.

在原帖中查看解决方案

3 回复数
1,917 次查看
stefancinipeanu
NXP Employee
NXP Employee

Hello, @esantana 

We have tested the ADC peripheral and we are not aware of any limitations. Did you try to run the ADC example on polling from MBDT IMXRT toolbox? What kind of error did you get when trying to build the application?

Usually, to use ADC in polling mode you just have to disable ADC interrupt from configuration file attached to the model, as depicted below:

stefancinipeanu_0-1673943997728.png

 

Best regards,

Stefan.

1,977 次查看
winter0147
Contributor I

Hello

I am just sharing here The MCUXpresso Config Tools are fully integrated into the MCUXpresso IDE, and also available as a standalone download for use with other supported IDEs, including Arm Keil, IAR EWARM and others. If using the MCUXpresso IDE, no additional download of Config Tools is required.

Hope so this information will help in resolving your  issue .

 

标记 (1)
0 项奖励
回复
2,010 次查看
Tyler691
Contributor I

The MIMXRT1170 SoC is configured to use the 24 MHz external oscillator on the board with the on-chip PLL to generate a 1 GHz core clock.

0 项奖励
回复