How to change default linker script

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to change default linker script

12,220 次查看
Maciek
Contributor V

Hi,

I'm using S32K1xx v4.1.0 toolbox. In the main Config block of the model after unchecking the 'Default Target Memory Definitions' I can see only 2 options to choose from:'S32K148_192_flash.ld' and 'S32K148_192_flash_bam.ld'. It does not matter what target MCU is selected. 

I've looked through installation catalog of MBD Toolbox - and there are multiple directories with linker script files. But I couldn't find one with only these two (visible in 'Config' block) linker scripts. 

How can I tell the MBD Toolbox to link using my custom linker script ?

Thanks
Maciek

0 项奖励
回复
13 回复数

11,735 次查看
Maciek
Contributor V

Hi again mariuslucianandrei,

after replacing the provided model in "...\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\mbdtbx_s32k" there is no change in behavior.

For example below is what I see after setting MCU to S32K116 (after saving/reopening model, selecting MCU again, changing it etc.). As You see other fields are re-populated correctly - only linker files are broken:

Nowy obraz mapy bitowej.bmp

I can still export the project to S32DS and change the linker to whatever I like - but it's a time consuming process and for quick prototyping the best solution is to change the linker script in Config block as intended in the Toolbox.

Thanks

Maciek

0 项奖励
回复

11,733 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello Maciek‌,

Sorry for my delayed response. We were pretty busy with the MPC release.

I have investigated more the issue you are encounter and this might be related to a callback.

Even if I can not reproduce the behavior and on my toolbox version the things seem to work fine, please once again, replace the following scripts and reply me if this solves this issue or not :smileygrin:.

  

Please replace the following scripts under S32K\src\mbdtbx_s32k\mscripts\config path

Hope this heps,

Marius

0 项奖励
回复

11,733 次查看
Maciek
Contributor V

Hi mariuslucianandrei,

after our previous failed attempt - I've returned to the original files - so now I've replaced/inserted files in the original installation. Two files were updated ('..._config_target_cbk' and '..._config_lcf_cbk'). The third file '..._config_populate_linker_files' was inserted in the same directory (I was not able to find such a file in the original installation). There is no change in behavior. I still can't see other linker files.

Please confirm that my procedure was ok. (for example I didn't use Your earlier updated '...ec_toolbox.mdl' file).

At the moment this problem is not very urgent for me. We've modified the original S32K144 linker file from the toolbox and left its original name. This way our modified linker file is taken into the build.

Much more urgent is the problem with failed download from the Simulink to the partitioned S32K144 (which I described in another forum post). We use EEPROM (with custom block library) and now after some minor update to the project, in order to check it on the EVB - I have to export it to the S32DS, set configurations by hand and test. If I have to do such task many times a day - it's very annoying. If You can - please look at this problem first !!!

Waiting for Your reply

Maciek

0 项奖励
回复

11,733 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello Maciek‌,

What's the name of your modified linker file? I am trying to understand why the toolbox does not display it.

Marius

0 项奖励
回复

11,733 次查看
Maciek
Contributor V

Hi mariuslucianandrei,

I've saved (backup) the oryginal 'S32K144_64_flash.ld' file from:

'...\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\mbdtbx_s32k14x\src\linker\gcc' folder.

Then I've modified the left 'S32K144_64_flash.ld' (assigning sections to FlexRAM). This way now the default linker file (which I can't change in the model config block) used by the toolbox (with it's default name unchanged) has all the modifications I need.

It's all happening in Matlab 2019b...

Maciek

0 项奖励
回复

11,733 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello Maciek‌,

Indeed the desired linker must be added in the S32K\src\mbdtbx_s32k14x\src\linker\gcc or another compiler if you need, respecting the following path [S32K1xx]_[flash size]_[flash/ram]_[desired name].ld 

Indeed, first I had the same issue when only the S32K148 was displaying, but closing and reopening the model and by reselecting the Controller from the MCU tab the rights Memory Definitions were selected. Unfortunately I couldn't reproduce it again. I assume this happens because of a callback or that ec_toolbox only contains those S32K148 linker files.

Also, the linkers used in our toolbox are the ones provided from the S32SDK. We only change a bit those ending with _bam, because of the requirements from the RAppId Bootloader.

Just to be sure. This might solve the question from Model on EVB doesn't start after re-partitioning for EEPROM ? Because I was thinking that the linker could be the problem but I had to check it.

pastedImage_1.png

Hope this helps,

Marius

0 项奖励
回复

11,733 次查看
Maciek
Contributor V

Hi mariuslucianandrei,

I'm not able to see other linker scripts. I've experimented with different scenarios like: saving model with unchecked option 'Default Target Mem...', closing and reopening again, switching between MCUs, selecting the same MCU again etc.

Nothing works - I can see only the two S32K148 linker scripts... In my Toolbox installation appropriate directories are filled with all linker scripts available (nothing is missing in the installation). For example in '...\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\mbdtbx_s32k14x\src\linker\gcc' folder I see 24 different linker scripts for all S32K14x parts.

It seems like some callback in the GUI that re-populates the list of available linkers is missing or doesn't work like intended.

In case of my other question: Model on EVB doesn't start after re-partitioning for EEPROM - I don't know if it has anything to do with the linker - because I didn't change the linker script at all. Default linker scripts (used by MBD Toolbox) don't allocate any sections to FlexNVM or FlexRAM.

Waiting for Your answer

Maciek

0 项奖励
回复

11,732 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello Maciek‌,

Let's update some files related with the linker files, under S32K\src\mbdtbx_s32k\mscripts\utils.

Indeed the linker file not specify any memory location for the FlexNVM or FlexRAM. is there any differences between the linker that we provide with the one from the S32DS project that you are using? Can you send me that linker file?

Hope this helps,

Marius

0 项奖励
回复

11,732 次查看
Maciek
Contributor V

Hi mariuslucianandrei,

I've found 'mbd_s32k_find_custom...' in the following folder:

"...\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\mbdtbx_s32k\mscripts\utils" and exchanged it with the provided new file.

I've found the other two files in the following folder:

"...\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx\mbdtbx_s32k\mscripts\config" and exchanged them with the provided new files. 

(Please note that my locations are a little different than Yours...)

And I can't see any difference. I've restarted Matlab, unchecked 'Default Target Mem...', reopened model, switch processors under 'MCU' tab etc. I still see only the 2 s32k148 linker scripts.

As to the linker file used with repartitioned device - it's the same linker script that is copied from Toolbox directory during 'Build' stage of the model to the model '_rtw' directory. After importing to S32DS this linker script is by default used in 

C/C++ Build->Settings->Tool Settings->Standard S32DS C Linker ->General->Script files. I was building in Simulink and in S32DS with standard Flash linker script.

I will put this part of the answer in the oryginal thread: https://community.nxp.com/thread/527793 

Waiting for response

Maciek

0 项奖励
回复

11,732 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello Maciek‌,

Since I can't really reproduce this error, I will provide the ec_toolbox  that has to be replaced here S32K\src\mbdtbx_s32k. Maybe the call of the callbacks is not right done.

If not I will change the script in order to display all the linker files in that folder.

I am sorry, the location you mentioned are right.

Hope this helps,

Marius

0 项奖励
回复

11,632 次查看
Maciek
Contributor V

Hi, https://community.nxp.com/t5/user/viewprofilepage/user-id/72088

we are working with S32K toolbox v4.2.0 for about 2 weeks now. I can confirm that exporting projects with referenced models to S32 Design Studio works now! (It didn't work in earlier version which was a big problem).

Unfortunately we still see the same problem with the custom linker files as before. This problem was NOT present immediately after the installation ! As I remember we have checked this on the 1st or 2nd day of using new version - and it was working ! We have been able to switch linker files as intended. 

Yesterday I've included new custom linker file into the appriopriate catalog and have tried to change the linker file in config. block - results the same as I've described at the start of this post. I always see only two S32K148 linker files (the two for default processor in config. block) - nothing else - independent of the choosen processor. And from this experience it looks like this feature is blocked at some point during using the tools. (we use the toolbox constantly).

Any new info about this ?

0 项奖励
回复

11,624 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello @Maciek ,

Thank you for reporting this behavior!

Indeed, this is very strange mainly because we do not block any feature in our toolbox after some time. Let me investigate this and I will reply here soon. 

Anyway, I will investigate this on R2019b (Is this the version of Matlab that you are using, right?) and reply here.

Regards,

Marius

0 项奖励
回复

11,618 次查看
Maciek
Contributor V

@https://community.nxp.com/t5/user/viewprofilepage/user-id/72088

We have installed (and are using) the toolbox v4.2.0 in Matlab R2020a.

Maciek