How do I use Freemaster for MBD toolbox MPC5744P rev2.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I use Freemaster for MBD toolbox MPC5744P rev2.0.0

2,399 次查看
erichsu
Contributor I

Hello Sir,

How do I use Freemaster for MBD toolbox MPC5744P rev2.0.0?

If  disable the freemmaster settings, CAN Bus can send messages normally,

The setting screen is as follows:

pastedImage_2.png

The error screen is as follows:

pastedImage_1.png

Could you help?

Thanks a lot.

Best Regards,

Eric

0 项奖励
回复
3 回复数

2,053 次查看
erichsu
Contributor I

Hi Daniel,

Freemaster CAN configuration is as follows:

pastedImage_1.png

My adapter is vector VN1630a in the list of supported devices, and show that communication could not be established after I clicked "Test connection" bottom .

The setting and error screen is as follows:

pastedImage_2.png

Looking forward for your reply.

Thanks a lot.

Best Regards,

Eric

0 项奖励
回复

2,053 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Eric, 

You have discovered a bug in the our setup.

I was able to reproduce the issue using this setup: MPC5744P evaluation board and IXXAT USB2CAN and the 500kb speed

1.JPG

I might have a quick and dirty fix for you until we will have a more stable hotfix. This fix works only with this setup which is similar with yours

2.JPG

Workaround:

- go to {toolbox install dir}\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\ folder and make a backup copy of mbdtargetmainlibpnt.tlc file

- copy and replace the file attached here in the {toolbox install dir}\mbdtbx_MPC574xP\mbdtbx_pnt\mbdtbx_pnt\ folder

- delete any previous generated model and build again the application.

Please confirm if it works or not in your case.

Thank you!

Daniel

0 项奖励
回复

2,053 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Eric, 

We need to know what we have done so far in terms of configuration.

From FreeMASTER/Project/Options you need to setup and configure the CAN communication.

Capture.JPG

Only some CAN drivers are supported. Is your adapter in the list of supported devices?

Capture.JPG

Looking forward for your reply.

Thank you!

Daniel

0 项奖励
回复