GDB server stuck, eval board MTRCKTSPS5744P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GDB server stuck, eval board MTRCKTSPS5744P

2,215件の閲覧回数
patel_reddy
Contributor I

Built project for eval board, MTRCKTSPS5744P, from inbuilt examples as per link in Getting Started with MTRCKTSPS5744P | NXP .

However during download process, the debug process stuck at 98%, ERROR seems to be at CRC mismatch.

pastedImage_2.png

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,067件の閲覧回数
patel_reddy
Contributor I

Looking at the debug code (pasted below), it seems to be a CRC check fail. Eval code has not been modified from project example. 

Loading programming algorithm ...
Done.
Programming sequency is : erase, blank check, program, and verify {default}
CMD>VC
Verifying object file CRC-16 to device ranges ...
block 00FA0000-00FA0007 ...
Ok.
block 01000000-01000291 ...
Calculated CRC-16 does not match block. (File = $06CF, Device = $79D8)
Current content of flash does not match application to be programmed

CMD>EM

Erasing.

0 件の賞賛
返信

2,067件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected] ,

In this community we mainly handle questions regarding MATLAB/Simulink and our toolboxes - I would recommend you try the https://community.nxp.com/community/s32/mpc5xxx community, where you'll most likely find answers to your question.

Kind regards,

Razvan.

0 件の賞賛
返信

2,067件の閲覧回数
patel_reddy
Contributor I
0 件の賞賛
返信