Freemaster (2.0.0.10) crashes when I click "variable watch" window

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster (2.0.0.10) crashes when I click "variable watch" window

1,353件の閲覧回数
senolgulgonul
Contributor II

S32DS is ok can upload flash

MATLAB coder is ok can embed into 5744p

Freemaster scope is working good, I enter variables from project-variables menu

Freemaster crashes If I click left or right mouse click on "varibale watch" window

0 件の賞賛
返信
2 返答(返信)

1,162件の閲覧回数
senolgulgonul
Contributor II

unfortunately this problem continues. I can connect to 5744p able to see scope and variable live but when I click into variable watch freemaster crashes with message "executable has stopped working"

windows 10

freemaster 2.0.8

freemaster 1.3 works fine but lack of many features, 1.4, 2.0.7 and 2.08 crashes when I click into "variable watch window"

0 件の賞賛
返信

1,162件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello senolgulgonul@gmail.com‌,

It seems to be a problem with the FreeMASTER itself. Can you share the Simulink model and FreeMASTER project you are running?

Note: you can try and update to the latest FreeMASTER - version 2.0.7.0 available here.

Kind regards,

Razvan.

0 件の賞賛
返信