Freemaster (2.0.0.10) crashes when I click "variable watch" window

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster (2.0.0.10) crashes when I click "variable watch" window

1,347 Views
senolgulgonul
Contributor II

S32DS is ok can upload flash

MATLAB coder is ok can embed into 5744p

Freemaster scope is working good, I enter variables from project-variables menu

Freemaster crashes If I click left or right mouse click on "varibale watch" window

0 Kudos
Reply
2 Replies

1,156 Views
senolgulgonul
Contributor II

unfortunately this problem continues. I can connect to 5744p able to see scope and variable live but when I click into variable watch freemaster crashes with message "executable has stopped working"

windows 10

freemaster 2.0.8

freemaster 1.3 works fine but lack of many features, 1.4, 2.0.7 and 2.08 crashes when I click into "variable watch window"

0 Kudos
Reply

1,156 Views
constantinrazva
NXP Employee
NXP Employee

Hello senolgulgonul@gmail.com‌,

It seems to be a problem with the FreeMASTER itself. Can you share the Simulink model and FreeMASTER project you are running?

Note: you can try and update to the latest FreeMASTER - version 2.0.7.0 available here.

Kind regards,

Razvan.

0 Kudos
Reply