Flash bootloader .rbf serial communication port for MPC5643L

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flash bootloader .rbf serial communication port for MPC5643L

跳至解决方案
1,885 次查看
Maciek
Contributor V

Hi,

I've managed to install MBD Toolbox for MPC564xL. I can build example models without problems. We have found older TWR-PXS2010 kit with PXS2010 which I know is earlier (before change) name for MPC5643L. 

Unfortuantely we don't have easy access to LINFlex_0 on this board. But LINFlex_1 can be accessed via on-board OSBDM Serial Bridge.

So I have a question:

is it possible to use Flash Bootloader (.rbf) for MPC5643L (or for PXS2010 - there is such .rbf in 'Bootloader' directory) with LINFlex_1 as serial communication interface ?

I can't find any info: what peripherals can be (are) used with this bootloader...

Thanks

Maciek

标记 (1)
0 项奖励
回复
1 解答
1,694 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Maciek‌,

The RAppID bootloader for MPC5643L MCU was built to support the communication over the LinFlex0 and CAN0.

These configurations are hard-coded inside the bootloader.

I do not know if that helps you - but that's how it was done.

Best regards,

Daniel

在原帖中查看解决方案

2 回复数
1,695 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Maciek‌,

The RAppID bootloader for MPC5643L MCU was built to support the communication over the LinFlex0 and CAN0.

These configurations are hard-coded inside the bootloader.

I do not know if that helps you - but that's how it was done.

Best regards,

Daniel

1,694 次查看
Maciek
Contributor V

Hi Daniel,

thanks for clarification. It helps.

It's strange but I really can't find reliable information how bootloaders are configured!

Thanks

Maciek

0 项奖励
回复