Firmware Update over CANFD with NXP MBDT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware Update over CANFD with NXP MBDT

1,947件の閲覧回数
viet
Contributor II

Hi all, 

FOTA ( Firmware Over The Air) is our requirement. 
one of the parts is distribute the firmware packages to another ECUs over CANFD (like BMS or OBC)

Does NXP MBD support firmware update over CANFD ?

if i does, please elaborate a bit more detail.

Thanks a lot for your support.

Viet

0 件の賞賛
返信
1 返信

1,916件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @viet, 

For this kind of code deployment, we are offering in our toolbox, both for the MPC and S32K the RAppID bootloader utility which can be used both over UART or CAN. But I don't think it uses CAN-FD.

To use it, you have to first flash the rbl bootloader file delivered with our toolbox, on the microcontroller using S32DS.

Then, in the model you have to select the Serial Download Interface option in the Target Connection tab of the Simulink config block. Once the code is automatically generated and built you have to open the RappID bootloader application and select the mot file, controller and the CAN probe.

This has been also discussed in this thread here https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Is-it-possible-to-use-MBDT-development-...

Hope this helps,

Marius

0 件の賞賛
返信