Example MBD Code of BLDC Trapezoidal Sensorless Control S12ZVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MBD Code of BLDC Trapezoidal Sensorless Control S12ZVM

2,297件の閲覧回数
tliu
Contributor I

Hi,

I wonder if there is any example mbd code for BLDC Trapezoidal sensorless control of S12ZVM available. I have some difficulty to implement the trapezoidal sensorless control into the mbd code. 

Thanks,

Tony 

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,166件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Tony, 

No, we do not have such example - BLDC Sensorless. 

What kind of issues are you facing ?

Best regards,
Daniel

0 件の賞賛
返信

2,166件の閲覧回数
tliu
Contributor I

Hi Daniel,

Thanks for the reply. My issue is about to measure the three phase voltage to get the back EMF, since there is a configuration block for GDU which set the GDUPHMUX to 00. I need to have GDUPHMUX changing between 01,10,11 to connect different phase to the adc to get the back EMF. Is there any method to achieve that? Thanks.

Best regards,

Tony

0 件の賞賛
返信