Error in donwloading the application to the S32K3X4EVB-T172 Board using MATLAB MBD toolbox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in donwloading the application to the S32K3X4EVB-T172 Board using MATLAB MBD toolbox

Jump to solution
4,053 Views
sagar991
Contributor II

I am trying to run the example s32k3xx_dio_s32ct on the S32K3X4EVB-T172 board, using NXP_MBDToolbox_S32k3xx version 1.4 on MATLAB 2023a. After changing the Hardware Part and the Communication port, the following error is occuring, "Problem occured while downloading the application on target". There is a runtime error.
See the attached pictures for more infomation on the error.


0 Kudos
Reply
1 Solution
3,842 Views
georgevictor
NXP Employee
NXP Employee

Hi, @sagar991,

You could try the solution proposed in this thread, Programming S32K344EVB-T172  and change the MATLAB Add-Ons folder location. The issue you are encountering may be related to the Windows path limitation.

Best regards,

Victor

View solution in original post

1 Reply
3,843 Views
georgevictor
NXP Employee
NXP Employee

Hi, @sagar991,

You could try the solution proposed in this thread, Programming S32K344EVB-T172  and change the MATLAB Add-Ons folder location. The issue you are encountering may be related to the Windows path limitation.

Best regards,

Victor