Does the Matlab Runtime work on NXP IMX8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does the Matlab Runtime work on NXP IMX8

跳至解决方案
2,182 次查看
RobertSheedy
Contributor I

We comile our Matlab code into a dll and run our production code using Matlab Runtime. THis is currently running on x86 hardware. We would like to run our production code on NXP iMX8 ARM processor. Is this possible?

标记 (1)
0 项奖励
回复
1 解答
2,170 次查看
brianmckay
Contributor III

Hi Robert,

The recommended / best way to get your MATLAB algorithm to run on IMX8 is to use the MathWorks Code Generation tools (MATLAB Coder and Embedded Coder). This converts your MATLAB algorithm into high-performance C /C++ code.  Then you use MCUXpresso (or IDE of you choice) to deploy on to the IMX8.

I don't think it is possible to run the Runtime on IMX8, and even if you could (maybe via some Linux tricks) I'd expect performance issues - modern MATLAB and the Runtime is not designed to run on embedded platforms, even one as advanced as IMX8. 

Cheers,

-Brian

在原帖中查看解决方案

1 回复
2,171 次查看
brianmckay
Contributor III

Hi Robert,

The recommended / best way to get your MATLAB algorithm to run on IMX8 is to use the MathWorks Code Generation tools (MATLAB Coder and Embedded Coder). This converts your MATLAB algorithm into high-performance C /C++ code.  Then you use MCUXpresso (or IDE of you choice) to deploy on to the IMX8.

I don't think it is possible to run the Runtime on IMX8, and even if you could (maybe via some Linux tricks) I'd expect performance issues - modern MATLAB and the Runtime is not designed to run on embedded platforms, even one as advanced as IMX8. 

Cheers,

-Brian