Does the Matlab Runtime work on NXP IMX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the Matlab Runtime work on NXP IMX8

ソリューションへジャンプ
2,929件の閲覧回数
RobertSheedy
Contributor I

We comile our Matlab code into a dll and run our production code using Matlab Runtime. THis is currently running on x86 hardware. We would like to run our production code on NXP iMX8 ARM processor. Is this possible?

タグ(1)
0 件の賞賛
返信
1 解決策
2,917件の閲覧回数
brianmckay
Contributor III

Hi Robert,

The recommended / best way to get your MATLAB algorithm to run on IMX8 is to use the MathWorks Code Generation tools (MATLAB Coder and Embedded Coder). This converts your MATLAB algorithm into high-performance C /C++ code.  Then you use MCUXpresso (or IDE of you choice) to deploy on to the IMX8.

I don't think it is possible to run the Runtime on IMX8, and even if you could (maybe via some Linux tricks) I'd expect performance issues - modern MATLAB and the Runtime is not designed to run on embedded platforms, even one as advanced as IMX8. 

Cheers,

-Brian

元の投稿で解決策を見る

1 返信
2,918件の閲覧回数
brianmckay
Contributor III

Hi Robert,

The recommended / best way to get your MATLAB algorithm to run on IMX8 is to use the MathWorks Code Generation tools (MATLAB Coder and Embedded Coder). This converts your MATLAB algorithm into high-performance C /C++ code.  Then you use MCUXpresso (or IDE of you choice) to deploy on to the IMX8.

I don't think it is possible to run the Runtime on IMX8, and even if you could (maybe via some Linux tricks) I'd expect performance issues - modern MATLAB and the Runtime is not designed to run on embedded platforms, even one as advanced as IMX8. 

Cheers,

-Brian