Does S12ZVMx Toolbox supports Matlab 2017a?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does S12ZVMx Toolbox supports Matlab 2017a?

2,252 次查看
jianlongzhang
NXP Employee
NXP Employee

Hi,

Customer reports that S12ZVMx Toolbox v1.3 is not compatible with Matlab 2017a. S12ZVM toolbox cannot be found in Simulink toolbox library. Would you please help to confirm if s12zvm toolbox could work on Matlab 2017a? thanks.

Best Regards

Tony Zhang 

4 回复数

2,001 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi faweiz‌,

Officially, the S12ZVMx Toolbox v1.3 was validated/tested on the following Matlab releases:  

- R2013A, R2013B, R2014A, R2014B, R2015A and R2015B
- 32-bit and 64-bit

Since the toolbox was released on November 27, 2015 - those were the only Matlab options at that time.

 

Nonetheless, the toolbox can be also installed on the 2017a and can be used for code generation.

The only option that "might" not work is the Processor-in-the-loop simulation due to changes in the Matlab environment.

In regards with the main question: "S12ZVM toolbox cannot be found in Simulink toolbox libraryi presume it is a simple to fix Matlab glitch.

Please have a look at this: https://community.nxp.com/message/915480?commentID=915480%23comment-915480#comment-911873 

Also, keep in mind that you:

1: need to successfully install a Toolbox license prior of seeing in it in the Simulink library;

2: need to execute the mcd_s12z_path.m script from toolbox root directory to setup the environment;

Hope this helps!

Daniel

2,001 次查看
ngoctuhoang
Contributor II

Hello Daniel,

"The only option that "might" not work is the Processor-in-the-loop simulation due to changes in the Matlab environment."

Maybe we have this problem with PIL under Matlab 2017a. Please See https://community.nxp.com/message/1339034 

Will MBD-toolbox for S12Z be developed/supported further or not? Because we have to decide whether we go with S12Z or not.

Thanks in Advance!

BR

Tony

0 项奖励
回复

2,001 次查看
Daniel_Popa
NXP Employee
NXP Employee

Screenshot with  S12ZVMx Toolbox v1.3 running under 2017a.

Capture.PNG

0 项奖励
回复

2,001 次查看
jianlongzhang
NXP Employee
NXP Employee

Hi Daniel,

Appreciate your prompt reply. I will inform customer and back to you if they have further issues. Thanks again.

Best Regards

Tony Zhang

0 项奖励
回复